SLUUCX0A February   2024  – June 2024 UCC57108

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  6. 2Hardware
    1. 2.1 Recommended Power Requirements
    2. 2.2 I/O Description
    3. 2.3 Jumper Description
    4. 2.4 Setup for Different UCC57108 Variants
    5. 2.5 DESAT Setup
  7. 3Implementation Results
    1. 3.1 Out-The-Box Evaluation
    2. 3.2 Equipment Setup
      1. 3.2.1 Power Supply
      2. 3.2.2 Function Generator
      3. 3.2.3 Oscilloscope
      4. 3.2.4 Digital Multimeter (DMM)
    3. 3.3 Bench Setup
    4. 3.4 Procedure and Results
  8. 4Typical Performance Waveforms
    1. 4.1 DESAT Feature
    2. 4.2 Bipolar Feature of UCC57108B
  9. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials
  10. 6Compliance Information
  11. 7Additional Information
    1. 7.1 Trademarks
  12. 8Revision History

Setup for Different UCC57108 Variants

The UCC57108EVM comes installed with the bipolar-voltage UCC57108B variant of the UCC57108 IC, and the EVM out-the-box is setup according to that variant. The UCC57108 family of devices comes in two more variants: the UCC57108C, which has split output, and the UCC57108W, which has enable function.

The UCC57108EVM also supports the UCC57102 IC, which is the 12.5V UVLO version of the UCC57108 IC. The UCC57102 has the same variant types as the UCC57108, and the information in this section applies to the UCC57102 IC as well. See the UCC5710x-Q1 High-Speed, Low-Side Gate Driver With DESAT Protection For Automotive Applications data sheet for more information.

Because each UCC57108 variant has slightly different pinouts, the EVM has jumpers to support the different variants. Jumpers J2 and J3 allow the user to short or open between connectors depending on which variant is being used. Figure 3-1 shows how J2 and J3 must be configured with each UCC57108 variant. Do not short more than one connection on J2. If the user is using variants other than the UCC57108B, then desolder resistor R16.

UCC57108EVM Jumper J2 and J3 Selection for
                    Each UCC57108 IC Variant Figure 2-1 Jumper J2 and J3 Selection for Each UCC57108 IC Variant

In addition to jumpers J2 and J3, there is also an option to solder 0Ω jumper resistors (R10, R12, or R16) for a low-parasitic way to short connections. The EVM out-the-box supports the UCC57108B variant, which has R16 installed on the board. Resistors R10 and R12 are not installed. If you are using the other variants, you must desolder R16. Table 3-4 to Table 3-6 showcases a guide to soldering or desoldering the 0Ω jumper resistors for each UCC57108 variant.

Table 2-4 Resistor Solder Guide for UCC57108B
R10R12R16
UCC57108BDesolderDesolderSolder
Table 2-5 Resistor Solder Guide for UCC57108C
R10R12R16
UCC57108CSolderSolderDesolder
Table 2-6 Resistor Solder Guide for UCC57108W
R10R12R16
UCC57108WDesolderSolderDesolder