The Board Offset calibration option is
not offered in Battery Management Studio, because the Board Offset calibration is
not required when using the BQ41Z50EVM.
- Connect and measure a -2A current
source from 1N (–) and Pack– (+) to calibrate without using the FETs. (TI does
not recommend calibration using the FETs).
- Enter –2000 in the Applied
Current field and select the Calibrate Current box.
- Press the Calibrate Gas
Gauge button to calibrate.
- Deselect the Calibrate Current
box after current calibration has completed.
Note:
Current can also be calibrated
using the FETs. Measure the current in the discharge path and enter this value
in the Applied Current field.