SLVA275C january 2010 – may 2023 UCD9081
Device Address Inputs: Shortly after the RST is negated, ADDR1-ADDR4 are sampled by the UCD9081 and define the 4 LSBs for device address on the I2C bus. The upper 3 bits of address are hardcoded at 0x6 giving an addressable range of 0x60-0x6F. These addresses are selected using pullup or pulldown resistors on the ADDRx inputs. Connecting ADDR1-ADDR4 to VSS locates the device at I2C address of 0x60; connecting ADDR1-ADDR4 to VCC locates the device at the I2C address of 0x6F. Once the ADDRx pins are sampled, they then function as EN/GPIO, and they are driven to their default inactive state as defined by the device configuration.