All trademarks are the property of their respective owners.
TPS613222A See References no. 1 is a very compact boost converter with only 3 active pins. Only two external components (one inductor and one output capacitor) are needed when designing a 5-V fixed output power rail. The quiescent is 6.5uA typically and the total power loss is very small even though the boost converter is always in active state. This part reduces the system cost significantly and makes the system design quite simple. But it has no short circuit protection.
TPS613222A is a hysteretic current control boost converter. There is a current comparator inside turns on and off the power MOSFETs. During the off-phase, the high-side MOSFET is on and the low side MOSFET is off. As the output voltage is higher than the input voltage, the inductor current ramps down. When the inductor current triggers the target value set by the output of the error amplifier, the high-side MOSFET is turned off and the low-side MOSFET is turned on (dead time control is integrated). Then the inductor current starts ramping up. When the inductor current ramps up to the target value set by the hysteretic current comparator, the low-side MOSFET is turned off and high-side MOSFET is turned on again. The TPS613222A operates in this behavior back and forth. If the output load goes beyond the TPS613222A’s capability, the peak switch current will be limited to 1.8A typically and the output voltage starts to drop. When the output voltage drops to the input voltage level, the inductor current is no longer controllable because even in off-phase, the inductor current ramps up not down and the boost converter may be damaged.
The technique used in this application note to achieve the short circuit protection adds two general purpose active switches and some passive components as shown in Figure 2-1. The resistor Rsense together with the Rds,on of the Q2 monitors the output current of the sub-system. The Vo- voltage is fed to the base of the NPN signal switch Q1. The Q1 is general purpose bipolar switch, for example, MMBT3904. When the Vo- ramps to the Vbe threshold of the Q1, which is 0.6 V typically, the collector current of Q1 increases significantly and pull the Vgs voltage of Q2 lower than the gate threshold voltage Vth. In this way, the current path is cut off immediately and both the power system and the sub-system is protected.
The short circuit current threshold ILIMIT is set by the Equation 1:
where
When the short circuit condition is removed, the Vo- voltage is pulled to GND slowly by the base-to-emitter current Ibe of the Q1. The recovery time is related to the output capacitor C3, and the leakage current set by Equation 2:
where
For example, the R2 is 1000 Ω, and the output capacitor is 4.7 µF. The Ileak is 4.4 mA, maximum. A simple 2.2-mA average leakage current can be used in the calculation. Then the recovery time is longer than 10 ms.
To accelerate the response time when SCP happens (or recovery time from SCP to normal mode), the resistor of R2 with smaller resistance can be used. The leakage current is inversely proportional to the R2 resistance according to the equation below. The recommended value for this resistor is between 100 Ω to 100 KΩ. It is a tradeoff between the recovery time/response time and the leakage current.
The following figures show the response time when a fast short-circuit accident happens. The Rsense is set to 0.5 Ω to get a 1.1-A target short-circuit current threshold. The actual trigger point is 1.1 A when the R2 is 100 Ω while the trigger point shifts to higher than 2 A when the R2 is higher than 10 kΩ.
The following explains how to select external components in such applications is another important topic. Especially the two external active switches.