Pay attentions to the following requirements:
- The maximum Vds voltage of the switch must be higher than the TPS613222A output voltage.
- If no Rsense, the Rds,on should also be balanced with the total solution efficiency, 3% is good tradeoff under the maximum load for the whole system power consumption.
- The maximum Vgs specification should exceed the maximum output voltage of TPS613222A under the worst condition.
- The parasitic capacitance is also problem for Q2. When a short circuit accident happens, the high slew rate di/dt introduces high spike at the drain-source of Q2. The maximum spike should not exceed the maximum V limitation.