SLVAE87A December 2020 – October 2023 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
AVDD, CVDD, and DVDD are regulated outputs derived from the LDOIN input. Each of these regulator outputs should have a bypass capacitor to avoid noise with a 10% tolerance due to the fact that a larger capacitance slows startup. REFHP is an internal reference voltage and NEG5V is a regulated voltage provided by an internal charge pump.
Each regulator provides power for delicate internal subsystems. Do not connect external circuitry or additional loads to these regulators beyond those described in the data sheet.
The bypass capacitors of the following pins shall be placed as close to the device pins as possible to ensure proper performance, especially the REFHP capacitor. It is also recommended to help performance with derating and emissions performance to utilize a small capacitor in parallel with each bypass LDO capacitor of 10-22%. For example, on CVDD, we recommend both a 22-nF and 100-nF capacitors in parallel with 4.7-μF decoupling capacitor to help reduce emissions. These need to be designed extremely close to the pins of the IC in the layout for best effect.