SLVAE87A December 2020 – October 2023 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
With the bus bar connected to a VC channel individually, the upper CB pin on that channel shall be left floating to avoid forward biasing the internal CBFET (see Figure 5-5 connection). This connection applies to the bus bar connecting to any middle VC channel individually. That is, in a single device, there is a cell connected above and below the VC channel with the bus bar connected.
To ensure hotplug performance, the CB channel where the bus bar is connected shall still have the differential capacitor CCB in Figure 5-5 , even if the upper CB pin is floating. This capacitor forms a complete capacitor ladder from all the cells and the bus bar connected to the device, allowing high voltage spikes during hotplug to be distributed across the capacitor ladder.
If the bus bar is connected to above the top of a module to an individual VC channel (see Figure 5-6 connection), the upper CB pin on that channel shall left floating, but the CB differential capacitor (CCB in Figure 5-6) shall still be connected. Additionally, an RC filter shall be connected from the top CB pin to the BAT pin. This additional RC filter (using the same RC values as the other RC filters on the CB pins) is to ensure a complete capacitor ladder. It is used to distribute high voltage spikes with the same RC constant as the rest of the CB pins during a hotplug event.