All other trademarks are the property of their respective owners.
Smart meters must continue to operate during brief power outages and send notification messages through a wireless radio, which consumes significant amount energy. As the output voltage of one cell supercap is not higher than 2.7 V, a boost converter is needed to step up the output voltage to power the GSM/GPRS module or MCU. The GSM/GPRS module voltage is normally higher than 3.6 V. The low input voltage boost converter can fully utilize the energy of the supercap and extend the backup power time.
The TPS61022 provides a power-supply solution for portable equipment and IoT devices powered by various batteries and super capacitors. The TPS61022 has minimum 6.5-A valley switch current limit over the full temperature range. With a wide input voltage range of 0.5 V to 5.5 V, the TPS61022 supports supercapacitor backup power applications, which may deeply discharge the supercapacitor.
Figure 1-1 is the schematic in the TPS61022EVM user’s guide designed for a 3.0 V to 4.2 V lithium-ion battery input, 5-V output power supply application. However, for low VIN of 0.5 V to 2.7 V supercap backup power application, an extra feedforward capacitor and big output capacitance is needed to increase the phase margin to make the loop stable.
This application report introduces how to select the TPS61022 external components for supercap backup power applications. Detailed calculation methods and bench test results are presented to verify the proposed circuit.
Figure 2-1 shows the theoretical circuit of the TPS61022 boost converter circuit in a supercap backup power system. The Vsys is the brief power, coming from other DC/DC converter or the grid. The TPS61022 has a MODE pin to set the operation mode. When the mode is logic high, the device operates at forced pulse width modulation (PWM) mode. At forced PWM mode, the device keeps switching with 1 MHz (VIN > 1.5 V) and 600 kHz (VIN < 1.0 V) disregarding the loading. This results in very low efficiency at light load conditions. There may be a reverse current from VOUT to charge the supercap by setting the MODE pin to logic high if the voltage of Vsys is higher than the TPS61022 setting output voltage. When the MODE is connected to a logic low voltage, the device works in auto PFM mode and there is no reverse current from VOUT to VIN by using the following configurations:
When the brief power Vsys browns out and drops less than the TPS61022 programmed output voltage VOUT, the TPS61022 starts switching and maintains VOUT at the programmed output voltage level.
To fully utilize the supercap energy and extend the backup power time, the TPS61022 device is used to regulate until the supercap voltage discharges to as low as 0.5 V. For low VIN < 1.5 V condition, TI recommends using a large output capacitance at TPS61022 output to lower the crossover frequency because the right half plane zero (RHPZ) frequency reduces with decreasing VIN.
where
Rout = output load resistor
D = duty cycle
L = inductance
For instance, when VIN = 0.7 V, VOUT = 3.3 V, IOUT = 0.8 A, L = 1 μH, fRHPZ = 29.5 kHz. It is generally accepted that the loop gain crossover no higher than the lower of either 1/10 of the switching frequency, ƒSW, or 1/5 of the RHPZ frequency, fRHPZ.
The TPS61022 Calculation Tool helps calculate the loop bode plot with 30-μF effective output capacitance by inputting the previously listed parameters. Figure 3-1 shows the crossover frequency is 6.2 kHz and phase margin is only 34.5°, which causes an unstable loop issue.
Therefore, to set the loop crossover frequency fc lower than 1/5 of the RHPZ frequency, a large output capacitance can decrease the crossover frequency. In the meantime, a feedforward capacitor (C3 in Figure 2-1) and resistor R3 in parallel with upper feedback resistor R1 introduces a pair of zero fFFZ and pole fZZP in the loop transfer function. By setting the proper zero frequency fFFZ, the feedforward capacitor can increase the phase margin to improve the loop stability. The pole fZZP can increase the phase margin by adjusting R3 resistance by Equation 2 and Equation 3.
Therefore, the ESR of the output capacitor creates a zero frequency:
Big ESR leads to a small zero fESR into the loop. Combining with the feedforward capacitor zero fFFZ, the crossover frequency fc will be increased to very high and phase margin is not big enough. Therefore, it is recommended to put a low ESR (< 50 mΩ) 100-µF aluminum electrolytic capacitor or aluminum polymer capacitor at the TPS61022 output. TI recommends setting the zero frequency fFFZ to 2 kHz. R3 is set to 2 kΩ in default, which helps eliminate the output AC noise coupled to the FB pin.