This application note presents ESD contact discharge test results for the TPS92630EVM, 3-channel LED driver, and demonstrates how ISO 10605 standards can be met for this device.
Automotive industry in-vehicle use cases:
All trademarks are the property of their respective owners.
A fully-compliant ESD chamber and equipment is used for this testing to conduct the following testing conditions.
The TPS92639EVM was protected with the ESD2CAN24-Q1, an automotive dual-ESD protection diode, soldered on the LED driver signal output and the LED loads of the evaluation module.
The following: