Water heaters are commonly used in daily life, the mechanism of which is similar to gas stoves. When ignition switch is triggered, fire is lit and the thermocouple is heated by the flame. At this time, a thermoelectric potential is generated, which in return will start the control system of the whole water heater, such as MCU. Therefore, the low voltage start up feature is preferred, cutting down the cost of selecting a thermocouple and the start-up time. Based on aforementioned application, an ultra-low voltage start-up scheme using BOOST converter TPS61299 is proposed in this application note.
All trademarks are the property of their respective owners.