SLVAFR6 January 2024 LM5067
According to this method, the LM5067 can be made to work normally in a larger dynamic voltage range by applying an external power supply VS, which solves the problem of the LM5067 under the traditional single negative power supply, eliminates the limit of the dynamic output voltage range of the chip caused by UVLO pin voltage limit. For further protection of the UVLO Pin pin, A TVS or Zener diode can be added between VEE pin and VIN pin for voltage clamping.