SLVAFR6 January   2024 LM5067

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2The External Auxiliary Power Supply and Op Amp Follows and Changes the UVLO Swing Amplitude of LM5067
  6. 3Testing and Verification
  7. 4Summary
  8. 5References

Abstract

In everyday life, there are many hot-swap scenarios. One of the hazards of hot-swap is that the transient rush currents and voltages generated by hot-swap can damage the post-stage circuitry. Hot-swap protection chips limit the transient power and transient current generated during hot-swap to protect the post-stage circuit. Hot-swap protection chips sometimes need to adapt to large dynamic range voltage swing, which can cause overstress on certain parameters of the chip during use. This paper proposes a method to add an auxiliary source. Theory and experimental verification can be used to extend the dynamic voltage operating range of this chip.