SLVK145 august   2023 TPS7H2201-SEP

PRODUCTION DATA  

  1.   1
  2.   Single-Event Effects Test Report of the TPS7H2201-SEP eFuse
  3.   Trademarks
  4. Introduction
  5. Single-Event Effects
  6. Device and Test Board Information
  7. Irradiation Facility and Setup
  8. Depth, Range, and LETEFF Calculation
  9. Test Setup and Procedures
  10. Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-Up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. Single-Event Transients (SET)
    1. 8.1 Single Event Transients
  12. Event Rate Calculations
  13. 10Summary
  14.   A References

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product were provided and delivered by the TAMU Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced Electron Cyclotron Resonance (ECR) ion source. At the fluxes used, 109Ag had good flux stability and high irradiation uniformity over a 1-in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic de-focusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For the bulk of these studies, ion flux of ≈ 105 ions/cm2·s were used to provide heavy-ion fluences of ≈ 107 ions/cm2 per run.

Figure 4-1 shows the TPS7H2201-SEP test board used for the experiments at the TAMU facility. Although not visible in this photo, the beam port has a 1-mil Aramica window to allow in-air testing while maintaining the vacuum within the accelerator with only minor ion energy loss. An in-air gap of 40-mm between the device and the ion beam port window was maintained at these distances for all runs respective to the ion that was tested.

GUID-20230811-SS0I-3MW4-L3TQ-XTVQ1ZSHBW73-low.svg Figure 4-1 Photograph of the TPS7H2201-SEP Evaluation Board Mounted in Front of the Heavy-Ion Beam Exit Port at the Texas A&M Cyclotron