SLVSER3A November 2018 – April 2020 TPS65982BB
PRODUCTION DATA.
The PP_5V0 path is unidirectional, only sourcing power from PP_5V0 to VBUS. When the switch is on, the protection circuitry limits reverse current from VBUS to PP_5V0. Figure 5 shows the I-V characteristics of the reverse-current protection feature. Figure 5 and the reverse-current limit can be approximated using Equation 1.