SLVSER3A November 2018 – April 2020 TPS65982BB
PRODUCTION DATA.
The VDDIO pin provides a secondary input allowing some I/Os to be powered by a source other than LDO_3V3. The default state is power from LDO_3V3. The memory stored in the flash configures the I/Os to use LDO_3V3 or VDDIO as a source. The application code automatically scales the input and output voltage thresholds of the I/O buffer accordingly. See the section for more information on the I/O buffer circuitry. See Table 4 for the recommended external capacitance on the VDDIO pin.