SLVU957A September 2019 – November 2021 BQ76922
The quick start guide describes connection for basic operation. Providing more than recognizable current in that configuration can require a power supply with a significant power rating. Applying a charge current can damage some power supplies. Figure 5-3 shows a method to force current through the sense path without a high wattage power supply or special equipment. The load power supply should be set at a low voltage in a constant current mode. Polarity can be reversed on the load supply to simulate a charge current. The battery simulation supply must never be reversed.