SLVU957A September 2019 – November 2021 BQ76922
The BQ76922 circuit module contains the BQ76922 IC and related circuitry to demonstrate the features of the IC. Surface mount FETs are provided for the high current path. A thermistor provides temperature sensing on the board. Other components provide support for the IC and connections to the board. Basic operation is described in the quick start guide. For details of the circuit, refer to the physical construction section.