SLVUAW9C September 2016 – February 2020 UCD90320
This command is used to turn outputs on and off along with input from the CONTROL pin. Section 12.1 of the PMBus specification describes this command in more detail.
The UCD90320 supports the following modes for the Operation command: