SLVUAW9C September 2016 – February 2020 UCD90320
This command, described in section 14.8 of the PMBus specification, is used to configure the gain of the current-sense circuit. The units for this command are milliohms (mV/A).
Note that some ambiguity exists in Rev 1.1 of the PMBus specification. One sentence says that the command uses the conductance of the sense resistor, but a later sentence says that the resistance must be used. In one place, the units are listed as ohms, but the default value is declared as 0 milliohms.
Rev 1.0 of the PMBus specification used resistance (not conductance) and milliohms. Rev 1.2 has cleared up this ambiguity and revert to the Rev 1.0 wording. For the UCD90320 devices, the ambiguous language in Rev 1.1 is interpreted to have the same meaning as Rev 1.0 (that is, milliohms).