SLVUAW9C September 2016 – February 2020 UCD90320
The following commands are replaced by the FAULT_RESPONSES command (see Section 10.23).
Code | Command |
---|---|
41h | VOUT_OV_FAULT_RESPONSE |
45h | VOUT_UV_FAULT_RESPONSE |
47h | IOUT_OC_FAULT_RESPONSE |
4Ch | IOUT_UC_FAULT_RESPONSE |
50h | OT_FAULT_RESPONSE |
63h | TON_MAX_FAULT_RESPONSE |