SLVUAW9C September 2016 – February 2020 UCD90320
This read-only, send byte common command returns the number of active pages. This value is determined by the MONITOR_CONFIG and SEQ_CONFIG commands (see Section 10.6 and Section 10.36). It is the higher page number derived from these two evaluations: