SLVUAW9C September 2016 – February 2020 UCD90320
This read/write word common command has two data bytes formatted in the Linear11 Data format. The units are percent change in how a millisecond is measured. The default value is 0.0%. Typical values are likely to be in the range from –2% to +2%. The command allows values from –100% to +99.9%. If the value returned from the RUN_TIME_CLOCK command (see Section 10.8) is slow, you use a negative percentage of the appropriate amount to correct it. If it is fast, you use a positive percentage. This command is not supported by UCD90320.