SLVUAW9C September 2016 – February 2020 UCD90320
Debug Function can be enabled with the input pin identified by this byte. The pin is ignored if the value of the byte is 0. Under Debug Mode, device shall not active PMBus alert pin for any faults/warnings, not response for any fault responses and not log any faults. This function is mainly designed for debug purpose and it is not recommended in the final production
The following faults/warnings are impacted by debug mode.
VOUT_OV_FAULT | TON_MAX | IOUT_UC | SYSTEM_WATCHDOG_TIMEOUT |
VOUT_OV_WARNING | TOFF_MAX Warning | OT_FAULT | SEQ_ON_TIMEOUT |
VOUT_UV_FAULT | IOUT_OC_FAULT | OT_WARNING | SEQ_OFF_TIMEOUT |
VOUT_UV_WARNING | IOUT_OC_WARNING | SLAVE_FAULT | RESEQUENCE_ERROR |
All GPI de-asserted |
When the debug mode is on, the rail sequence on/off dependency conditions are ignored, as soon as the sequence on/off timeout is expired, the rails will be sequenced on or off accordingly regardless of the timeout action, if the sequence on/off timeout value is set to 0, the rails will be sequenced on or off immediately. The fault pin shall not pull the fault bus low when debug mode is on. Moreover LGPOs affected by these events should be back to their original states when debug mode is on. System watchdog function is disable when debug mode is on.