10.36.3 GPI Sequence Off Dependency Mask
Each of the 32 pages has its own GPI Sequence Off Dependency Mask, whose bits are defined as follows:
Bit |
31 |
30 |
29 |
28 |
27 |
26 |
25 |
24 |
Purpose |
GPI31 |
GPI30 |
GPI29 |
GPI28 |
GPI27 |
GPI26 |
GPI25 |
GPI24 |
Bit |
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
Purpose |
GPI15 |
GPI14 |
GPI13 |
GPI12 |
GPI11 |
GPI10 |
GPI9 |
GPI8 |
GPI7 |
GPI6 |
GPI5 |
GPI4 |
GPI3 |
GPI2 |
GPI1 |
GPI0 |
Bit |
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
Purpose |
GPI15 |
GPI14 |
GPI13 |
GPI12 |
GPI11 |
GPI10 |
GPI9 |
GPI8 |
Bit |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
Purpose |
GPI7 |
GPI6 |
GPI5 |
GPI4 |
GPI3 |
GPI2 |
GPI1 |
GPI0 |
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
GPI15 |
GPI14 |
GPI13 |
GPI12 |
GPI11 |
GPI10 |
GPI9 |
GPI8 |
GPI7 |
GPI6 |
GPI5 |
GPI4 |
GPI3 |
GPI2 |
GPI1 |
GPI0 |
The enable pin for the page is not de-asserted until all of the input pins selected by the GPI bits are de-asserted. Once the enable pin is de-asserted, the state of these GPI pins has no effect on the state of the enable pin.
Each page can depend on the state of up to thirty-two input pins. The same pins can be used to control multiple pages. (see Section 10.39)