SLVUAW9C September 2016 – February 2020 UCD90320
Each of the 32 pages has its own GPO Sequence Off Dependency Mask, whose bits are defined as follows:
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
GPO15 | GPO14 | GPO13 | GPO12 | GPO11 | GPO10 | GPO9 | GPO8 | GPO7 | GPO6 | GPO5 | GPO4 | GPO3 | GPO2 | GPO1 | GPO0 |
The enable pin for the page is not de-asserted until all of the pins selected by the GPO bits are de-asserted. Once the enable pin is de-asserted, the state of these GPO has no effect on the state of the enable pin.
Each page can depend on the state of up to sixteen GPO. The same GPO can be used to control multiple pages. (See Section 10.38)