SLVUAW9C September 2016 – February 2020 UCD90320
The latched status types (_LATCH) in the GPO_CONFIG command can be cleared by a pin. That Input Pin is selected by this byte (see Table 66). The pin is ignored if the value of this byte is 0. This pin is edge-sensitive.