SLVUBT8B November 2020 – June 2022 LP8764-Q1 , TPS6594-Q1
The PMIC GUI is based upon GUI Composer which is compatible with either Chrome™ (version 46+) or Firefox™ (version 38+). The Chrome™ web browser is recommended and used throughout this document for demonstration. The GUI is found through the TI Development tools at TI DevTools page. Navigating to the Gallery from the Explore tab, highlighted in red in Figure 5-1, is one way to enter the Gallery.
When in the gallery, locate the Scalable PMIC's GUI panel shown in Figure 5-2. If the panel is not visible on the main page, then use the search bar and enter the term PMIC.