SLVUBT8B November 2020 – June 2022 LP8764-Q1 , TPS6594-Q1
This migration example continues to use the Generic_LP8764 with the required changes to the json file as described in Section 15.1.
As described in section Section 8.1.2.1, the PFSM_START state is required and must be added. In the Generic_LP8764 example, the STANDBY state can be entered from either the ACTIVE or MCU_ONLY states and therefore a separate state for PFSM_START must be added as shown in Figure 15-3. If the STANBY state has no inputs from other states and is designated as the start state, then it is possible to simply rename the STANDBY state to PFSM_START.