SLVUCD1A May 2022 – September 2024 TPS65219 , TPS65219-Q1
The PMIC GUI is based upon GUI Composer which is compatible with either Chrome® (version 46+) or Firefox® (version 38+). The Chrome web browser is recommended and used throughout this document for demonstration. The PMIC GUI is also compatible with Microsoft Edge® (as of version 111.0.1661.41). The GUI is found through the TI Development tools at TI DevTools page. Navigating to the Gallery from the Tools tab, highlighted in blue in Figure 6-1, is one way to enter the Gallery.
In the gallery, locate the TPS65219_GUI panel shown in Figure 6-2 by using the search bar and entering TPS65219_GUI.