SLVUCF3 March 2022 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , LP8764-Q1 , TDA4VM , TDA4VM-Q1 , TPS6594-Q1
This section provides examples of how to interact with the PMICs from the perspective of the MCU and over I2C. Table 7-1 shows how the I2C commands are presented in the following sections. These examples, when used in conjunction with the datasheet, can be generalized and applied to other use cases.
I2C Address | Register Address | Data | Mask | |
---|---|---|---|---|
Write | 0x48 or 0x4C | 0x00 - 0xFF | 0x00 - 0xFF | 0x00 - 0xFF |
Read | 0x48 or 0x4C | 0x00 - 0xFF | NA | NA |