SLVUCL3 December   2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Cautions and Warnings
  4. 2Introduction
  5. 3Quick Start Guide
  6. 4Hardware and Software Overview
    1. 4.1 Hardware Connections Overview – DRV8317HEVM + LAUNCHXL-F280049C
    2. 4.2 Connection Details
    3. 4.3 LED Lights
    4. 4.4 DRV8317HEVM Configurability – Jumpers and Resistors
      1. 4.4.1 DRV8317H Compatibility
      2. 4.4.2 DRV8317S Compatibility
      3. 4.4.3 MCU Power Options
      4. 4.4.4 Interfacing DRV8317HEVM and LAUNCHXL-F280049C LaunchPad
  7. 5Hardware Setup
  8. 6Firmware and GUI Application
    1. 6.1 C2000 InstaSPIN Universal GUI
    2. 6.2 Motor Identification
    3. 6.3 Sensorless-FOC Commutation
    4. 6.4 Torque Control, Speed Control, and Advanced Modulation Techniques
    5. 6.5 SPI Communication (DRV8317S only)
  9. 7Schematics
    1. 7.1 Main Supply
    2. 7.2 DRV8317H/S
    3. 7.3 3.3V Buck Regulator and VREF
    4. 7.4 26
    5. 7.5 LaunchPad Connections
    6. 7.6 Connectors & Interface
    7. 7.7 Status LEDs, Voltage Sense, and Protection
  10. 8Revision History

Hardware Setup

The hardware required to run the motor control is the LAUNCHXL-F280049C LaunchPad development kit, the DRV8317HEVM, a Micro-USB cable, and a power supply with a DC output from 4.5-V to 20-V. Follow these steps to set up the evaluation module:

  1. Check that all resistors or jumpers are set up accordingly according to the device variant used. The DRV8317HEVM by default is populated with and configured for the DRV8317H (hardware variant). If using the DRV8317S, please populate the resistors mentioned in row I of Table 4-2 to configure the board for the proper device variant.
  2. Mate the DRV8317HEVM board to the top half of the LAUNCHXL-F280049C LaunchPad development kit (mates to J1/J3 and J2/J4 of LaunchPad, as in Figure 4-3).
    Note: Observe the correct orientation when placing DRV8317HEVM to the LAUNCHXL-F280049C. The motor and power connectors will face to the LaunchPad’s Micro-USB connector.
  3. Connect the three phases from the brushless-DC motor to the 3-pin connector J6 on DRV8317HEVM. Phases OUTA, OUTB, and OUTC are labeled in white silkscreen on the PCB top layer.
    Note: If using a sensored algorithm on the LaunchPad development kit, connect Hall sensors to the 5-pin connector J7.
  4. Connect the DC power supply to header J5.
    Note: Observe the correct polarity for the VBAT and GND connections on the DRV8317HEVM connector J5.
  5. Connect a Micro-USB cable to the LaunchPad development kit and computer.
  6. Turn on the power supply and power up the PCB.

If using the DRV8317HEVM with an external microcontroller, make the connections needed on the male headers on the top of the board or female connectors on the bottom side of the board.