SLVUCQ6 july 2023 TPS7H2211-SEP
The TPS7H2211EVM is the Evaluation Module (EVM) for the plastic package option of the TPS7H2211 and provides a platform to electrically evaluate the features. This user’s guide provides details about the EVM, including the configuration, schematics, and BOM.
The EVM is designed to be used across the entire input voltage and output current range of the TPS7H2211 while providing flexibility in configuring the device under different conditions. By default, the device in the EVM is configured as shown in TPS7H2211EVM Default Configuration. To configure the device in a different configuration, please refer to the TPS7H2211 data sheet to calculate the values of the passives around the device that needs to be changed.