SLVUCR9B August 2023 – January 2024 TPS2HCS10-Q1
The EVM kit for the HSS-HCMOTHERBRDEVM includes the following:
The kit for the daughter cards are specific to the high-side switch associated with the daughter card. An example kit contents for the HSS-2HCS10EVM daughter card can be seen below:
Note that in addition to daughter cards with silicon pre-soldered, TI offers a "blank" daughter card called HSS-HCS-BLANKEVM. This blank daughter card is useful when running destructive tests and can be used with any compatible HCS high-side switch.