SLVUCV6 May 2024 TPSM81033
4*22µF ceramic capacitors are used in the EVM, the effective capacitor value is approximately 20µF. If the load current is smaller than 1A, then 2*22uF ceramic capacitor (effective capacitor value is approximately 10µF) is also proper.