Prior to connecting the input power source, set
the current limit of the input supply to 0.1A
maximum. Make sure the input source is initially
set to 0V and connected to the J1 terminal as
shown in Figure 3-1.
Connect voltmeter 1 at VIN+ and VIN– test points
to measure the input voltage.