3 Quick Start Setup and Use
The following instructions are to set up and use the TMAG5123EVM:
- Power up the EVM using either of the following methods:
- USB power:
- Insert the micro USB cable into the EVM onboard USB receptacle J1.
- Plug the USB cable into any USB power source (for example: laptop, desktop, power bank, and so forth).
- Variable power supply
- Set the power supply voltage to desired setting between 2.5 V and 38 V. Do not turn on the power yet.
- Connect the power supply V– terminal to the black GND test point on the EVM.
- Connect the power supply V+ terminal to the red VCC test point on the EVM.
- Turn on the power supply.