To set up the GUI the first time,
follow these steps:
- Make sure that the above mentioned
driver was installed successfully to verify that everything works properly and
that the GUI can update the EVM firmware, if necessary.
- With the EVM/TI-SCB Controller unit
plugged to the PC, go to the GUI link: https://dev.ti.com/gallery/search/TMAG6180-6181.
- To launch the GUI from the web
browser, click the GUI Composer application to open the GUI
Composer window (see Figure 3-8).
- For first-time GUI Composer
setup, follow the prompts to download the TI Cloud Agent and
browser extension (see Figure 3-9). These prompts appear after you close the README.md
dialog.
- Optionally, click the
icon in the GUI Composer window to download
the GUI for offline use (see Figure 3-8).