If the EVM does not work as expected,
use the Figure 7-1 to
identify potential root causes. Consider the following:
- Do not make modifications to the
EVM or change the default settings until AFTER it is verified to be
working.
- Register read back requires the
correct software setup, See Section 3.2.2 for details.
- The POR current of the
LMX2571EPEVM is approximately 30 mA.
- The power-down current of the
LMX2571EPEVM is approximately 3 mA.