SNAU296 December 2023 LMK5C33414A
Another option is to feed an external clock to the XO SMA port (J8) to drive the XO input. See Figure 3-9. This path can be connected to the XO input pins. Y1 needs to be powered down when using the external XO input path. To power down Y1 and use an external XO input, the jumper on JP4 must be removed. Suggested XO frequencies for best device performance are frequencies of 38.88 MHz and 48 MHz. When using an external XO input, TI recommends to remove the capacitor (C71) connecting the TCXO output to the XO input of the LMK5C33414A. This prevents any risk of backdriving the onboard TCXO.