- The following scenario is used when the
device that is being used for the receiver already contains a termination resistor. The
process and the equations are roughly the same with just a few adjustments due to the added
resistance. Ensure that the receiver being used contains a termination resistor and obtains
the value of the resistance from the data sheet.
- If your device does contains internal
termination, then the equations shown in Figure 4-1 will be used.
- For the simulation, the following values
will be used:
- VCC = 3.3 V
- VA = 1.2 V, LVDS driver
output fixed common mode voltage
- VB = 0.9 V, Sub-LVDS driver
output fixed common mode voltage
- RE = 50Ω
- RT = 100Ω, value of
termination resistor inside device
- Using the formulas a, b, and c from Section 2 creates a system of
equations in order to solve for the resistance values that will best fit the desired
parameters for Sub-LVDS. The following values were obtained from the system of equations:
- R1 = 222Ω
- R2 = 32Ω
- R3 = 95Ω
Proceed to simulate the circuit in order to
verify the correct behavior.
Note: Resistors R7 and R8
are used to imitate the high impedance inputs of a receiver.
- The simulation shown in Figure 4-3 demonstrates a voltage swing of approximately:
- VID ≈ 160 mV
- VOD ≈ 325 mV
- VID falls within the desired
range. If the formulas are used to obtain values for VID, VCMF, and
RE with the resistor values and the measured values for VOD and
VA then we obtain the following results:
- VID = 163 mV
- VB = 0.9 V
- RE = 50Ω