SNLA420A September 2022 – January 2024 DP83TC812R-Q1 , DP83TG720S-Q1
Another benefit of some Base-T1 PHYs is the ability to conduct diagnostics of the interface during data communication. Using a diagnostic tool requires a media access control interface to provide full access to the serial management interface of the PHY.
These are the current integrated diagnostic features of the TI PHYs:
For more details, see the diagnostic tool kit section of the DP83TG720S-Q1 1000BASE-T1 Automotive Ethernet PHY with SGMII and RGMII data sheet.
Base-T1 Ethernet technology features, such as low cable count and high bandwidth, can enable real-time diagnostic capability, including cable diagnostics that can detect when a cable is damaged or degrading. This detection feature allows engineers to replace cables during normal maintenance instead of performing production-line stops.