SNLA426 june 2023 DS320PR1601 , DS320PR410
Trace length matching between different lanes or pairs is not required. An embedded clock within each differential pair allows for different differential trace length. However, there is a limit to prevent ASIC buffer over-flow. Typically, there can be up to 1 inch of difference, but this depends on the data rate and PCB board material.
Intra-pair trace – the trace length of positive versus negative lead of the signal – has to be kept within 5 mils. This is done to minimize common mode noise. This becomes even more crucial to consider when vias are present in the signal path of a differential pair. Match the etch lengths of the relevant differential pair traces of each interface. The etch length of the differential pair groups do not need to match (that is, the length of the transmit pair does not need to match the length of the receive pair).