The following section describes the
steps needed to install the Texas Instruments SigCon Architect GUI and the
DS320PR410 SigCon Architect GUI profile.
- Download and install the Texas
Instruments SigCon Architect GUI EVM v3 program. Follow the steps in the
SigCon Architect: Installation and Starter’s
Guide for detailed instructions.
- Download and install the
DS320PR410 SigCon Architect GUI Profile Updater from the TI website or secure
resource folder.
- Connect a USB2ANY Interface Adapter or Aardvark I2C Host Adapter to
the desired DS320PR410 and PC.
- Launch the SigCon Architect EVM
GUI v3 program and make sure that the DS320PR410 profile has been installed.
When successfully installed, the program is shown as an instance of the
DS320PR410 device below the Selection column of the SigCon
Architect GUI.
Descriptions of each DS320PR410 SigCon
Architect GUI page are listed in the following:
- Configuration Page: Used
to configure device SMBus/I2C Addresses, device EVM model, number of
devices (in DS320PR410EVM-CUSTOM mode only), and interface adapter.
Note: The
Configuration Page page must be configured before accessing any
of the additional GUI pages.
- Low Level Page: Individual
register access to each device. This page can be used to change specific
register settings or to verify that changes from the High Level Page have
taken effect.
- EEPROM Page: Used to
create, read, and write EEPROM Hex files (following Intel™ Hex format). When the DS320PR410 is
configured in SMBus/I2C primary mode (MODE = L1), the redriver loads
the settings stored in an external EEPROM upon power-up. The user can configure
these settings using this page.
- High Level Page: Main page
used to change EQ settings (EQ Index/CTLE, DC Gain) of the device and to monitor
the active status of each channel.
- Eye Height Page: Used to
perform an EyeScan of selected channels and display the EyeScan
result plot in graphical form. This can assist in tuning the DS320PR410 and
choosing an EQ Index for your system. Please refer to the Eye Scan with TI
PCI-Express Gen5.0 Redrivers application note for further
details.