Shielded cable surge test with direct contact
on cable shield:
- Verify the surge injection point is properly connected to the shield
- Verify there is no discontinuity on the shield of the cables
- Point of noise injection needs to be at least 10cm away from the DUT and LP
Shielded cable surge test with CDN connector:
- Verify both side of the Ethernet cable matches
- Verify the CDN and Ethernet cable type match
- Using unshielded cable CDN with shielded cable mismatch can
potentially increase reflective noise due to the discontinuous
ground in the signal lines.
- Using unshielded cable CDN with shielded cable can also increase the
impedance of the return path between signal lines and earth ground
which can increase the noise ratio done by surge test
- Verify the Noise injection
CDN is properly connected to the earth ground
- Verify both DUT and LP are away from the CDN connector
- Longer cable is preferred on
the link partner side
- Longer cable on the
link partner side can reduce some effect of surge noise done to the
link partner
General test setup procedure:
- Verify surge noise injection cable is straight, without loops
- Verify the Ethernet cable is placed properly on the insulator, and does not
contact earth ground
- Verify the Ethernet cable is
placed away from any noise sources
- Add a good return path from
the RJ45 shield to earth ground
- Verify there are no loops on
the Ethernet cable to reduce cross talk
- Use shielded cable for better EMI performance:
- Having a shielded
cable is better than non-shielded cable, as the shielded cable
provides a path from MDI lines to ground through cable shield or
decoupling capacitors inside shielded cable CDN
- For non-shielded
cables, all noise can go directly to signal lines with minimal or no
noise coupling to ground