SNOA963B February 2020 – July 2021 LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
Tuning button sensitivity requires a correctly configured LDC211x/LDC3114. The configuration process(3) prior to tuning the button activation force should include the following:
A quick way to check whether the device is configured correctly is by probing the INx pins; the waveforms should resemble those shown in Figure 3-1.
An error-free STATUS (Register 0x00) and correct sensor frequency, sampling window, and scan rate are good indications of a correctly configured LDC211x/LDC3114. Once the device has been verified to have been configured correctly the gain can be adjusted for each individual button by following these steps:
The SWITCHINGTHRESHOLD can be calculated using Equation 2.
where
The GAINnFACTORNEW needs to be now correlated back to the closest GAINn decimal value using Table 41 in the LDC2114 data sheet and programmed into the corresponding GAINn register.
If the above process was followed correctly the button should now be calibrated to the desired button activation force. As an additional quality check, one can program the LDC211x/LDC3114 with the calculated gain factor, apply the desired button activation force, and verify if the button turns on. Section 4 walks through an example of the threshold configuration process for an inductive touch button interface.