SNOA993A June 2018 – July 2021 LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
The maximum supported continuous button actuation is ~50 seconds. If the button is asserted for a longer time interval, the device internal state machine automatically resets operation and the baseline tracking value automatically resets, which deasserts the button. When a timeout occurs, the device will flag the event by setting STATUS:TIMEOUT to 1.
For the LDC3114, the baseline tracking algorithm may be disabled by using the device in raw data access mode.