SNOAA90A february 2023 – may 2023 DRV5033-Q1 , LDC3114-Q1 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1
With vehicle electrification on the rise, there is a business need to replace electro-mechanical devices in automotive designs. Many interaction points in a vehicle require some kind of button, dial, or switch to register user input. These interaction points can be designed under a variety of new technological implementations that allow more design freedom than the traditional electro-mechanical applications. This paper discusses different HMI applications commonly used in vehicles and the different technologies that can be used to implement these applications.
All trademarks are the property of their respective owners.