SNOU164B September 2018 – June 2024
The TLV40x1EVM quadrant is assembled with the TLV40x1 device, a 0.1µF ceramic capacitor (in 0603 package), and a 100kΩ pull-up resistor (only for Quadrants I and II). If the application needs to scale down the input voltage to a lower value, a pair of resistors R1 and R2 can be installed by the user. In this case, connect the voltage to be monitored to IN_AUX (DIP PIN 7) instead of IN (DIP PIN 8).
Depending on the user’s setup or requirement, a standard 8-pin DIP socket or 0.1-inch pin headers can be installed. Users can also solder wires directly to the DIP holes.