SNOU200 October   2024 LMH6518

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1 Preliminary Setup
    2. 2.2 Basic Operation
    3. 2.3 Jumper Information
    4. 2.4 SPI
    5. 2.5 Logic Function Description
    6. 2.6 Header Information
  8. 3Hardware Design Files
    1. 3.1 Schematic
    2. 3.2 PCB Layouts
    3. 3.3 Bill of Materials (BOM)
  9. 4Additional Information
    1. 4.1 Trademarks

Preliminary Setup

The LMH6518 is easily configured with the USB2ANY interface adapter. The USB2ANY product page provides the required software and a detailed user’s guide for the adapter. The USB2ANY Explorer Software can be found under the Order & start development tab on the product’s homepage. The user’s guide, found under the Technical Documentation tab, highlights the general setup and operation of the adapter. The USB2ANY is shipped with a USB cable, a 10-pin cable, and a 30-pin cable. For communication with the LMH6518 evaluation board, the 10-pin cable is used as well as the USB cable to interface with the computer.

Once the software is installed follow the procedures below to configure the adapter to interface with the evaluation board.

  1. Open USB2ANY Explorer software and confirm the device is recognized when plugged into the computer using the USB cable. Users receive a message in the activity log confirming the controller was connected successfully.
    LMH6518EVM USB2ANY Detection ConfirmationFigure 2-1 USB2ANY Detection Confirmation
  2. Click the Select Interfaces and check the box next to SPI.
    LMH6518EVM Adding SPI Tab to GUIFigure 2-2 Adding SPI Tab to GUI
    LMH6518EVM Selecting SPI InterfaceFigure 2-3 Selecting SPI Interface
  3. Click on the SPI tab and select the settings as shown below that correspond to the LMH6518 SPI functionality.
    LMH6518EVM SPI TabFigure 2-4 SPI Tab
    LMH6518EVM SPI ConfigurationFigure 2-5 SPI Configuration
  4. Set byte number to 3 bytes that corresponds to LMH6518 SPI communication length.
    LMH6518EVM Setting Bytes for SPI CommunicationFigure 2-6 Setting Bytes for SPI Communication
  5. Plug the 10-pin cable in the appropriate orientation into the USB2ANY adapter. The key on the 10-pin cable lines up with the USB2ANY.
    LMH6518EVM USB2ANY 10-Pin HeaderFigure 2-7 USB2ANY 10-Pin Header
  6. Plug the other end of the ribbon cable into J2 of the LMH6518 evaluation board with the cable key on the side of the key label on the board.