SNVA966 July 2020 – MONTH LP8864-Q1 , LP8864S-Q1 , LP8866-Q1 , LP8866S-Q1
If the ISET pin resistor is shorted to GND during normal operation, the maximum current for each LED channel can be calculated in the following equation:
LED_CURRENT[11:0] register will be written to 1/4 of latest programmed data through I2C. The default value of LED_CURRENT[11:0] register is 0xFFF if it is not programmed after device enabling. If ISET pin voltage returns back to above 1.1 V, the LED_CURRENT[11:0] register data is written to latest programmed data through I2C. The ISET_STATUS fault bit will be set in the BOOST_FAULT_STATUS register and the INT pin is triggered.